High Current Implanters

  1. VIIsta 3000XP - HE14 / (IMPV14-01) - Implanter 300mm

    High Current Implanters

    VIIsta 3000XP - HE14 / (IMPV14-01) - Implanter 300mm

    Available: Immediately

    The equipment is currently still in warm SteelTypeVIIsta 3000XPWafersize300mmCE MarkYesConnection top/bottomtopLabel KitGerman

  2. AMAT E500

    High Current Implanters

    AMAT E500

    › Original Equipment Manufacturer? (Yes/No, if no please state the details ) Yes› Exact Model Type? (Yes/No, if no please state the details ) E500 EHP› OEM Serial ID?ES193741 U2› Completeness: Total/partial/Donor tool? Please list missing parts.Total› Date of first usage?NA› Technic special customized for Infineon?NA› Correct maintained?Yes› Any damages/deficits known?No› Manuals existing?No› Crated: If yes…/ professional with protocol / partly / simple?No› Detailed Configuration/Specification of the tool › Any upgrades / extensions?Thin Wafer handling kit, Hydrogen implant, LX upgrade, Windown 7 OS› Useable for which products?8"  Thin Taiko wafers› Wafer size (if applicable)?200mm› Any consumables at end of lifetime?Yes (source, electrode)› Procured from OEM or from second hand?From IR Singapore› Any refurbishments done?No› Was there a significant system failure in the last three years?No› Any contaminations known?BF3, H2› IFX inventory200016809location INFINEON KULIM FAB 2 LEVEL 3 PRODUCTION AREA CLEANROOM
  3. Varian Kestrel 1520 - Tool as spares bundle

    High Current Implanters

    Varian Kestrel 1520 - Tool as spares bundle

    Tool is 98% complete but has many special Infineon optimizations/modifications.

    Therefore we recommend this tool as spares-donor-tool. The tool is still installed and ready for inspection in our site Kulim.2)      Headline & DescriptionKestrel 15203)      How many units14)      Manufacture (if applicable)Varian Semiconductor5)      Condition (Very Good/like New/Never Used/Good/Fair/Poor)Good6)      Year of manufacture 20127)      W X H X D in cm276 x 227 x 6328)      Weight25800kg9)      Purchase Date201210)   Purchase Cost167132.2511) Net Book Value 12)   Function (New – Never used/Working/Tested Needs Repair/ Needs Repair/ Untested/System Incomplete )Tested need Service13)   Appearance (New/Like New/Excellent/Very Good/Good/Poor?)Very good14) LocationKulim15) FE/BE (FE/BE/Unknown)?BE  Additional details › Original Equipment Manufacturer? (Yes/No, if no please state the details ) No, modified to run Hygrogen beam for Infineon› Exact Model Type? (Yes/No, if no please state the details ) Kestrel 1520› OEM Serial ID?ES184258› Completeness: Total/partial/Donor tool? Please list missing parts.total› Date of first usage?2011 at IFKM› Technic special customized for Infineon?Yes, modified as proton implanter by Infineon› Correct maintained?Yes› Any damages/deficits known?machine failed to boot up, CPU and machine no linking› Manuals existing?Yes› Crated: If yes…/ professional with protocol / partly / simple?No› Detailed Configuration/Specification of the toolmidified to run Hydrogen beam, GC wafer› Any upgrades / extensions?no› Useable for which products?field stop› Wafer size (if applicable)?200mm› Any consumables at end of lifetime?yes, machine EOS in year 2018› Procured from OEM or from second hand?relocation from IFAT› Any refurbishments done?No› Any doubts that the tool is failure free useable for the next three years?NA, EOS machine› Was there a significant system failure in the last three years?only CPU failure› Any contaminations known?no, only run hydrogen gas