Ion Implantation Equipment

  1. VIIsta 3000XP - HE14 / (IMPV14-01) - Implanter 300mm

    High Current Implanters

    VIIsta 3000XP - HE14 / (IMPV14-01) - Implanter 300mm

    Available: Immediately

    The equipment is currently still in warm SteelTypeVIIsta 3000XPWafersize300mmCE MarkYesConnection top/bottomtopLabel KitGerman

  2. Axcelis NV8250HT #941

    Medium Current Implanters

    Axcelis NV8250HT #941

    Equipment Konfiguration: Type:NV8250HTEnergy Config:0 - 250Kv MidcurrentSerialnumber:908Build Year:2002Date of first usage:buyed new from vendorCurrent Condition: GoodCE-Conformity:YesLocation:greyroomVoltage:208VCryo-Pumps:3x CTI/Edwards Onboard: OB-8Cryo-Kompressor:CTI 9650 Low-VoltageTurbo-Pumps:Seiko/Edwards: STP1003C, STP-301C, STP-1003CRough-Pumps:Edwards: without QDP40, not includedEndstation Rough-Pump:not includedWafersize:8inch(200mm)Clamp-Type:E-Chuck green with Non-µC ControllerWafer-Cooling:Galden HT110 with Affinity PWC-020K-BE35CBD2 (R507) (condition unclear)Gasbox:Modular 5-String, 4x 2,0L SizeString1:Argon Carriergas; MFC Unit-1662 2sccm BF3String2:BF3 SDS-Low-Pressure Type VCR 1/4"; MFC Unit-1662 2sccm BF3String3:condition unclear, Type VCR 1/4" MFC Unit-1662 2sccm BF3String4:AsH3 SDS-Low-Pressure Type VCR 1/2"; MFC Unit-1662 2sccm BF3String5:PH3 SDS-Low-Pressure Type VCR 1/2"; MFC Unit-1662 2sccm BF3Beam-Profiler Type:Belt-DriveGear-Type's:Scan: Planetary  Tilt: PlanetarySource-Type:ELS4 IHC-Source without VaporizerHV-Transformer:Silicon-OilLight-Tower:red/yellow/green; no buzzerMain-WorkstationSolaris SUN AXI 4HE PH: 200978Second-WorkstationSolaris SUN Sparc5Software-Version:5.1.4.1Network:24port 100MB Ethernet with Cisco Router-KitCell-Controller:177 TypeNotes:Upper-Rack Panel missing Clean-Room Table missing on frontside all 4 wheels on oil-isolation transformer are broken Minor modifications on tool No Manual-Set/ no Spares include tool was used 24/7 full in production between 15 and 230kv Energy If required, tool can be inspected on site, but no Power
  3. AMAT E500

    High Current Implanters

    AMAT E500

    › Original Equipment Manufacturer? (Yes/No, if no please state the details ) Yes› Exact Model Type? (Yes/No, if no please state the details ) E500 EHP› OEM Serial ID?ES193741 U2› Completeness: Total/partial/Donor tool? Please list missing parts.Total› Date of first usage?NA› Technic special customized for Infineon?NA› Correct maintained?Yes› Any damages/deficits known?No› Manuals existing?No› Crated: If yes…/ professional with protocol / partly / simple?No› Detailed Configuration/Specification of the tool › Any upgrades / extensions?Thin Wafer handling kit, Hydrogen implant, LX upgrade, Windown 7 OS› Useable for which products?8"  Thin Taiko wafers› Wafer size (if applicable)?200mm› Any consumables at end of lifetime?Yes (source, electrode)› Procured from OEM or from second hand?From IR Singapore› Any refurbishments done?No› Was there a significant system failure in the last three years?No› Any contaminations known?BF3, H2› IFX inventory200016809location INFINEON KULIM FAB 2 LEVEL 3 PRODUCTION AREA CLEANROOM
  4. Varian Kestrel 1520 - Tool as spares bundle

    High Current Implanters

    Varian Kestrel 1520 - Tool as spares bundle

    Tool is 98% complete but has many special Infineon optimizations/modifications.

    Therefore we recommend this tool as spares-donor-tool. The tool is still installed and ready for inspection in our site Kulim.2)      Headline & DescriptionKestrel 15203)      How many units14)      Manufacture (if applicable)Varian Semiconductor5)      Condition (Very Good/like New/Never Used/Good/Fair/Poor)Good6)      Year of manufacture 20127)      W X H X D in cm276 x 227 x 6328)      Weight25800kg9)      Purchase Date201210)   Purchase Cost167132.2511) Net Book Value 12)   Function (New – Never used/Working/Tested Needs Repair/ Needs Repair/ Untested/System Incomplete )Tested need Service13)   Appearance (New/Like New/Excellent/Very Good/Good/Poor?)Very good14) LocationKulim15) FE/BE (FE/BE/Unknown)?BE  Additional details › Original Equipment Manufacturer? (Yes/No, if no please state the details ) No, modified to run Hygrogen beam for Infineon› Exact Model Type? (Yes/No, if no please state the details ) Kestrel 1520› OEM Serial ID?ES184258› Completeness: Total/partial/Donor tool? Please list missing parts.total› Date of first usage?2011 at IFKM› Technic special customized for Infineon?Yes, modified as proton implanter by Infineon› Correct maintained?Yes› Any damages/deficits known?machine failed to boot up, CPU and machine no linking› Manuals existing?Yes› Crated: If yes…/ professional with protocol / partly / simple?No› Detailed Configuration/Specification of the toolmidified to run Hydrogen beam, GC wafer› Any upgrades / extensions?no› Useable for which products?field stop› Wafer size (if applicable)?200mm› Any consumables at end of lifetime?yes, machine EOS in year 2018› Procured from OEM or from second hand?relocation from IFAT› Any refurbishments done?No› Any doubts that the tool is failure free useable for the next three years?NA, EOS machine› Was there a significant system failure in the last three years?only CPU failure› Any contaminations known?no, only run hydrogen gas