ITEM ID: 265759

Varian Kestrel 1520 - Tool as spares bundle

Tool is 98% complete but has many special Infineon optimizations/modifications.

Therefore we recommend this tool as spares-donor-tool. The tool is still installed and ready for inspection in our site Kulim.2)      Headline & DescriptionKestrel 15203)      How many units14)      Manufacture (if applicable)Varian Semiconductor5)      Condition (Very Good/like New/Never Used/Good/Fair/Poor)Good6)      Year of manufacture 20127)      W X H X D in cm276 x 227 x 6328)      Weight25800kg9)      Purchase Date201210)   Purchase Cost167132.2511) Net Book Value 12)   Function (New – Never used/Working/Tested Needs Repair/ Needs Repair/ Untested/System Incomplete )Tested need Service13)   Appearance (New/Like New/Excellent/Very Good/Good/Poor?)Very good14) LocationKulim15) FE/BE (FE/BE/Unknown)?BE  Additional details › Original Equipment Manufacturer? (Yes/No, if no please state the details ) No, modified to run Hygrogen beam for Infineon› Exact Model Type? (Yes/No, if no please state the details ) Kestrel 1520› OEM Serial ID?ES184258› Completeness: Total/partial/Donor tool? Please list missing parts.total› Date of first usage?2011 at IFKM› Technic special customized for Infineon?Yes, modified as proton implanter by Infineon› Correct maintained?Yes› Any damages/deficits known?machine failed to boot up, CPU and machine no linking› Manuals existing?Yes› Crated: If yes…/ professional with protocol / partly / simple?No› Detailed Configuration/Specification of the toolmidified to run Hydrogen beam, GC wafer› Any upgrades / extensions?no› Useable for which products?field stop› Wafer size (if applicable)?200mm› Any consumables at end of lifetime?yes, machine EOS in year 2018› Procured from OEM or from second hand?relocation from IFAT› Any refurbishments done?No› Any doubts that the tool is failure free useable for the next three years?NA, EOS machine› Was there a significant system failure in the last three years?only CPU failure› Any contaminations known?no, only run hydrogen gas

1 unit @ $149,000.00

MAKE: Varian

MODEL: KESTREL 1520

CONDITION: Good

CATEGORY: High Current Implanters

YEAR: 2012

Kulim, Malaysia

SPECS

Manufacturer Varian
Model KESTREL 1520
Condition Good
Year of Manufacture 2012

S&H

All items are sold on condition `as is and where is`. Ex work from current location excluding de-installation, de-hook up, discharge, packaging, crating and delivery. We are not responsible for any damage incurred during shipment.

Payment

100% downpayment